Navigate to cross references for alarm input and target tags
Find cross references for alarm input tags and target tags.
To navigate to cross references for alarm input and target tags
- On theController Organizer, expand theAlarm Managerfolder, and open theAlarmslist.
- To navigate to the cross reference for an alarm input tag, right-click an alarm and selectGo To Cross Reference For Input Tag <input tag name>. The input tag for an alarm drives the alarm state.
- To navigate to the cross reference for an alarm target tag, right-click an alarm and selectGo To Cross Reference For Target Tag <target tag name>. The target tag for an alarm is a tag that is used to evaluate the alarm's condition.
Provide Feedback