Delete a zone

Deleting a zone
removes all devices, conduits, and endpoints
assigned to the zone.
Prerequisites
To retain the devices from the zone to delete, assign devices to different zones or unassign the devices from zones. If needed, recreate the conduits.
  1. To delete a zone
  2. From the navigation bar, select either
    Canvas
    or
    Zones
    .
    TIP: In
    ZONES
    , select
    Overview
    to see all zones in a table.
  3. Right-click the zone to delete and select
    Delete
    .
    NOTE: To delete multiple zones, either:
    • In
      ZONES
      , hold
      , select multiple zones, and then select
      Delete
      next to any selected zone.
    • In
      Overview
      , hold
      , select multiple zones, and then select
      Delete
      from the toolbar.
  4. Select
    DELETE
    .
The zone is no longer a part of the policy model.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal