Delete a range

Delete a range of trusted IP addresses that you no longer need.
  1. From the navigation bar, either:
    • Select
      Canvas
      .
    • Select
      Zones
      and then select a zone that contains the range.
    • Select
      Devices
      .
  2. Right-click the range to delete and select
    Delete
    .
    NOTE: To delete multiple ranges, hold
    , select multiple ranges, and then select
    Delete
    from the toolbar.
  3. Select
    DELETE
    .
The range is deleted and is no longer a part of the policy model.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal