Search discovered devices

Use
Discovery
to search for a device to determine its location. After the initial discovery of the network topology, you can use filters to limit the scope of the search.
When using search, take a note of these functional details:
  • Search only examines devices detected or viewed by the browser. Initiating a search will not cause the browser to discover a new device.
  • Search queries can contain alphanumeric characters, full words, compound expressions, fragments of a word, or a single letter or number.
  • Search includes predefined search criteria to filter search results by device, name, path, and IP address.
  • Enclose search queries in quotation marks to find exact matches.
  • Use operators in the search query to refine the search results using a logical statement.
    • AND
      to search for two or more keywords.
    • OR
      to search for several keywords.
      TIP:
      An example of using operators between keywords to refine search results is:
      Device: 1756-L OR Device: 1768-L
      This search locates both ControlLogix and CompactLogix controllers.
  • Clear the search query to return to the network topology tree view.
  1. To search discovered devices
  2. In
    Discovery
    , select either
    CIP
    or
    OPC UA
    .
  3. (CIP only) From the
    Discovery
    toolbar, select
    Search
    .
  4. In
    Search
    or
    Filter
    , enter a query.
  5. (optional, CIP only) Select a search filter by selecting
    to narrow the search results to:
    Device
    The name of the device. For example,
    1756-L
    Address
    The IP address or a portion of the IP address of the device: For example,
    10.122.155
    OnlineName
    The online name of the device. For example,
    Packaging line
    Location
    The communications path used for the device: For example,
    AB-Eth
Discovery
displays results within a few seconds, regardless of pressing
.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal