Configure automatic device discovery

Enable or disable the automatic discovery of CIP or OPC UA devices in the
Discovery
pane.
  • To enable the automatic discovery of CIP devices:
    1. In
      Discovery
      , select
      CIP
      .
    2. Select
      Auto browse
      to enable or disable the automatic discovery of CIP devices.
  • To enable the automatic discovery of OPC UA devices:
    1. In
      Discovery
      , select
      OPC UA
      .
    2. Select
      Auto browse
      to enable or disable the automatic discovery of OPC UA devices.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal