Bridge networks

Bridge networks to create conduits between networks.
  1. From
    Discovery
    , on the
    CIP
    tab, select
    Settings
    .
  2. On the
    Bridged
    tab, select
    + Add New
    .
  3. In
    Name
    , enter a name for the bridge.
  4. Next to
    Selected Target Bridge Network
    , select
    Browse
    .
  5. Either:
    • To create a bridge path, in
      Bridge Path Selection
      , select the network to connect the current network and then select
      OK
      .
    • To add an existing bridge path from another bridge, select
      Copy Setting From
      and select a configuration.
  6. Select
    OK
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal