Delete a conduit

Delete a conduit to remove a connection between two endpoints.
  1. From the navigation bar, select
    Conduits
    .
  2. Right-click the conduit to delete and select
    Delete
    .
    NOTE: To delete multiple conduits, hold
    , select multiple conduits, and then select
    Delete
    from the toolbar.
  3. Select
    DELETE
    .
The conduit is no longer part of the policy model.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal