Restore a policy model

Restore
FactoryTalk System Services
to return the
FactoryTalk System Services
databases to a known good state.
  1. Verify the
    backup.zip
    file is present in this location
    C:\ProgramData\Rockwell\RNAServer\Global\RnaStore\FTSS_Backup
  2. Open the command prompt as an Administrator.
  3. In the command prompt, enter
    cd "C:\Program Files (x86)\Rockwell Software\FactoryTalk System Services"
  4. Run the
    FactoryTalk System Services
    Backup & Restore Utility by entering either:
    • Policy model from a plaintext backup. Enter
      FTSSBackupRestore -R
    • Encrypted backup. Enter
      FTSSBackupRestore -R -P "password"
      or
      FTSSBackupRestore -R -P password
      Restores an encrypted backup that is decrypted using the password supplied after the
      -P
      parameter. Quotation marks are optional.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal