Back up a policy model
Back up
FactoryTalk System Services
to save a copy of the policy model and its associated certificates.- Open the command prompt as an Administrator.
- In the command prompt, entercd "C:\Program Files (x86)\Rockwell Software\FactoryTalk System Services"
- Run the backup utility by entering one of these commands:
- To create a plaintext backup of the data, enterFtssBackupRestore -B
- To create an encrypted backup of the data, enterFtssBackupRestore -B -PorpasswordFtssBackupRestore -B -P "password"Creates an encrypted backup of the data using the password supplied after the-Pparameter. Quotation marks are optional. This password must be supplied to restore the data.
Thebackup.zipfile is created. Once performed, theFactoryTalk Services PlatformBackup includes this file. - Verify that the backup file is present in this locationC:\ProgramData\Rockwell\RNAServer\Global\RnaStore\FTSS_BackupTIP: TheProgramDatafolder is hidden by default inWindowsFile Explorer.
Provide Feedback