Policy model example

The policy model example includes three zones connected with conduits that contain different device types.
Policy model example
Policy model example
Diagram description - policy model example
Item
Name
Description
1
CIP and OPC UA
zone
Contains
OPC UA
devices and
CIP
devices.
2
Secure
conduit
Connects
CIP and OPC UA
zone with
OPC UA
zone.
3
Trusted unsecure
conduit
Connects
OPC UA
zone with
CIP Security
zone.
4
OPC UA
zone
Contains
OPC UA
devices only, including two
OPC UA
clients and one
OPC UA
server.
5
CIP Security
zone
Contains three
CIP
devices.
6
Onboarding Area
container
Contains devices found by Automatic Policy Deployment that can be added to the policy model.
There are no devices found by Automatic Policy Deployment in this example.
7
Unassigned
container
Contains devices added to the policy model but not added to any zone in the policy model.
There are two unassigned devices in this example.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal