Policy model auditing
FactoryTalk System Services
generate diagnostic messages upon specific actions and
log them to FactoryTalk Diagnostics
. These messages can be later reviewed as a part of an
audit.Message categories
The diagnostic messages are divided into these categories:
- Model deployment
- Sent when you deploy a security policy model or cancel deployment.
- Model creation
- Sent when you create a security policy model.
- Model editing
- Sent when you edit the security policy model.
Provide Feedback