CIP Bridging settings hierarchy
The CIP Bridging settings can be global or specific to a port, device, or
zone.
Settings levels
The following list outlines the CIP bridging settings levels (from the lowest level to the highest level):
- Port-level settings
- Zone-level settings
- FactoryTalk Policy ManagerSettings
The CIP Bridging settings
follow these conventions:
- The lower-level settings must be compliant with the higher-level settings.
- The lower-level settings can be stricter than the higher-level settings.
- If the lower-level settings are less strict than the higher-level settings, the higher-level settings overwrite the lower-level settings.
Port-level settings
These settings apply to EtherNet/IP interfaces and provide the distinction between secure
and Trusted IP (permitted) traffic.
TIP:
During the initial policy deployment,
FactoryTalk Policy Manager
attempts to identify the modules that occupy chassis
slots.Device-level settings
These settings enable or disable the communication bridging between the USB port of a device and a backplane or other physical ports.
Zone-level settings
These settings ensure compliance for all port-level and device-level settings. The port-level and device-level settings can be stricter than zone-level settings.
The following table shows examples of zone-level settings paired with port-level settings:
Zone settings | Port settings | Description |
---|---|---|
Inbound CIP bridging
Outbound CIP bridging
| Inbound CIP bridging
Outbound CIP bridging
| Allowed configuration. The port-level settings (lower-level settings) and zone-level settings (higher-level settings) match. |
Inbound CIP bridging
Outbound CIP bridging
| Inbound CIP bridging
Outbound CIP bridging
| Allowed configuration. The port-level settings (lower-level settings) are stricter than the zone-level settings (higher-level settings). |
Inbound CIP bridging
Outbound CIP bridging
| Inbound CIP bridging
Outbound CIP bridging
| Disallowed configuration. The port-level settings (lower-level settings) are less strict than the zone-level settings (higher-level settings). |
Settings
Global policy ensures compliance for all zones in the model. The zone-level settings can be
stricter than
FactoryTalk Policy Manager
Settings.The following table shows examples of
FactoryTalk Policy Manager
Settings paired with
zone-level settings:FactoryTalk Policy Manager Settings | Zone Settings | Description |
---|---|---|
Inbound CIP bridging
Outbound CIP bridging
| Inbound CIP bridging
Outbound CIP bridging
| Allowed configuration. The port-level settings (lower-level settings) and zone-level settings (higher-level settings) match. |
Inbound CIP bridging
Outbound CIP bridging
| Inbound CIP bridging
Outbound CIP bridging
| Allowed configuration. The zone-level settings (lower-level settings) are stricter than the Model
Settings (higher-level settings). |
Inbound CIP bridging
Outbound CIP bridging
| Inbound CIP bridging
Outbound CIP bridging
| Disallowed configuration. The zone-level settings (lower-level settings) are less strict than the Model
Settings (higher-level settings). |
Provide Feedback