Configure a recipes editor
Configure the recipes editor to manage recipes at runtime.
- From the toolbar, select.Template Libraries
- InTemplate Libraries, selectWidgets.
- DragRecipes Editorto theUIfolder inProject view.
- InProject view, create an instance ofRecipesEditor (type).
- InProperties, inRecipeSchemaAliascreate a dynamic link with theRecipe Schemaobject.
- (Optional) InProperties, configure theAppearance,Size and layout, andEvents.
Provide Feedback