Configure an alarm grid

Add a table that displays alarms status in real time.
  1. From the toolbar, select
    Template Libraries icon
    Template Libraries
    .
  2. In , search for
    Alarm Grid
    .
  3. Under
    Components
    , drag
    Alarm Grid
    onto
    Page2 (type)
    in
    Project view
    .
    AlarmGrid1
    appears under
    Page2 (type)
    .
  4. Select
    Close
    .
  5. In
    Project view
    , select
    AlarmGrid1
    .
  6. In
    Properties
    , set
    Horizontal alignment
    to
    Stretch
    .
    The object adjusts its width to the container at runtime.
AlarmGrid1 in Page2
Alarm grid interface with columns for timestamp, name, source variable, message,
            active status, acknowledgment, confirmation, and severity. Four buttons labeled
            Acknowledge, Acknowledge All, Confirm, and Confirm All display below the grid.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal