Configure a widget to display logged alarms

Add a widget that displays historical data about alarms at runtime.
  1. From the toolbar, select
    Template Libraries icon
    Template Libraries
    .
  2. In , search for
    Alarm History Grid with filter
    .
  3. Under
    Components
    , drag
    Alarm History Grid with filter
    onto
    Page3 (type)
    in
    Project view
    .
  4. Select
    Close
    .
  5. In
    Project view
    , select
    FilteredAlarmHistoryGrid1
    .
  6. In
    Properties
    , set
    Horizontal alignment
    to
    Stretch
    .
    The object adjusts its width to the container at runtime.
  7. Create a dynamic link between
    AlarmsEventLogger
    and
    ProjectName
    Loggers
    AlarmsEventLogger1
    .
    For more information about dynamic links, see Create dynamic links.
Filtered Alarms History Grid with filter in Page3
Alarms interface showing columns for timestamp, name, source variable, message,
            active, acked, confirmed, and severity. The interface includes date and time filters and
            a refresh button.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal