Develop an icon that changes color
Configure an image of a conveyor that changes chassis color based on the associated alarm state.
NOTE:
Download a sample project:
ChangeIconColorBasedOnAlarm.zipApplication example - disabled alarm
![](/content/dam/dita/en/factorytalk-optix/current/_images/ChangeIconBasedOnAlarm1.png/_jcr_content/renditions/original)
Application example - enabled alarm
![](/content/dam/dita/en/factorytalk-optix/current/_images/ChangeIconBasedOnAlarm2.png/_jcr_content/renditions/original)
Prerequisites
- To develop the project
- Arrange the interface elements.
![](/content/dam/dita/en/factorytalk-optix/current/_images/ChangeIconBasedOnAlarmDesign.png/_jcr_content/renditions/original)
Select
to run the project using the client emulator to test your project. To run the project on a remote client, see Add a client device.
Run
Provide Feedback