Configure a native presentation engine

Create a native presentation engine if you run
FactoryTalk Optix
as an application on the local device. For a typical HMI scenario, this directly renders the
FactoryTalk Optix Application
on the screen of the target device.
  1. In
    Project view
    , right-click the
    UI
    folder and select
    New
    Native presentation engine
    .
  2. In
    Properties
    , make any necessary changes:
    • Dynamic variables polling time
      . Time interval between variable readings.
    • Text render type
      . Specify how text renders to the UI control.
    • Web browser local content policy
      . Either load remote resources in the web browser from locally hosted pages or not.
    • LoginWindow
      . Login window type that displays at session start if no user is logged in.
    • Virtual keyboard
      . Select the default virtual keyboard. See Keyboards.
    • Start window
      . Window object type created at the start of a session.
    • Starting user
      . User that authenticates the session.
    • Style sheet
      . Style graphic objects.
    • Session
      . UI Session object to use. See UI session.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal