Key-value editor
Use the key-value editor to configure key-value pairs for dynamic link
conversion. Access the editor in advanced dynamic link editor.
TIP:
Open the key-value editor by selecting
next to the key-value converter in advanced
dynamic link editor.


Item | Name | Description |
|---|---|---|
![]() | Converter path | The path to the converter. |
![]() | ![]() | Adds a key-value table row. |
![]() | Delete | Deletes the selected key-value table row. |
![]() | Data type | Indicates the data type of keys or values. Select to choose a
different data type. |
![]() | Key | A converter key (source value). |
![]() | Value | A value that corresponds with the key in the same row (output
value).
TIP:
The value in the first row is the
default value. If the source value does not correspond with any
converter key, the converter returns the default value.
|
Provide Feedback