Configure a recipe

Create a recipe schema that uses the Ingredient01, Ingredient02, and Ingredient03 variables.
  1. From the toolbar, select
    Open dashboard page
    .
  2. In the editor, select
    Configure a recipe
    .
  3. Select
    New recipe
    .
  4. Create a dynamic link between
    Target node
    and:
    • If you created variables,
      ProjectName
      Model
      .
    • If you imported Logix controller variables,
      ProjectName
      CommDrivers
      LogixDriver1
      LogixStation1
      Tags
      Controller Tags
      .
  5. Select
    Next
    and select
    Next
    .
  6. Select
    New database
    .
  7. In
    Name
    , enter
    RecipeDB
    and select
    Next
    .
  8. Select
    Next
    and select
    Next
    .
  9. Select
    Ingredient01
    ,
    Ingredient02
    , and
    Ingredient03
    , and select
    Next
    .
    Selected variables
  10. Select
    Exit
    .
In
Project view
,
RecipeSchema1
appears under
Recipes
.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal