Push changes to a remote repository

Push changes that you make to a remote repository to back up the project to a location other than your local computer and provide version control for the project. Changes pushed to the remote repository are available to others who work on the project.
When there are changes to push, the message "Local changes are available to push" appears in the status bar and the
Push to remote
icon displays a blue number with the number of commits to push.
IMPORTANT: When you push changes to the remote repository, the project must be synchronized or you will be prompted to pull from the remote repository and resolve conflicts. When there are changes to pull, the message "Local and remote changes available to push and pull" appears in the status bar and 
Pull from remote
displays a blue number with the number of commits to pull. 
  1. From the open project, select
    Push to remote
    .
    If you do not have a
    FactoryTalk Optix Studio
    user identity you are are not authorized to push changes to the remote repository.
    Push to remote
    displays "No identifies have been configured." Select
    Configure Provider identity
    and to configure the identity, see Set options.
  2. (optional) If version control is enabled for a local project and you are pushing changes from the local project the first time and a remote repository is not yet associated with the project, in
    Push to remote
    , configure a remote repository:
    1. Identity
      . Select your identity. This can be either your
      GitLab®
      or
      GitHub®
      identity.
    2. Owner/Group
      . Select the owner or group of the repository. This can be either your identity or a group to which you belong.
    3. Private
      . Select to create a private repository that only the selected owner or group can associate with a project.
    4. Public
      . Select to create a public repository that other owners and groups can associate with a project.
    5. URL
      . Displays the URL of the repository based on the selected settings.
    6. Select
      Push to remote
      to create a new repository or use an existing repository that is empty.
    TIP: In order to use version control, FactoryTalk Optix project names and repository names must match. The project and repository names must contain only alpha numeric characters, numerals, periods, dashes, and underscores.
The changes are pushed to the repository and "Project synchronized" appears in the Status bar.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal