Configure a scale layout

To configure a scale layout, add a scale layout object and child objects and then change the properties of the scale layout.
  1. In
    Project view
    , right-click the node to contain the scale layout object and select
    New
    Containers
    Scale layout
    .
    For example, add the scale layout under
    MainWindow (type)
    .
  2. (optional) Hover-over the scale layout, select
    Edit
    , and then enter a custom name for the object.
  3. Add or move child graphic objects under the scale layout.
    For more information on how to move graphic objects, see Move a node.
    For example, add buttons under the grid layout to create a grid of buttons. See Button.
  4. In
    Project view
    , double-click the scale layout object, and in
    Properties
    , complete:
    • Fill Mode
      . Select
      Fit
      to keep the original aspect ratio of child objects when you resize the scale layout object; Select
      Stretch
      to disregard the original aspect ratio of child objects when you resize the scale layout object.
    • Font scaling
      . Scale the font size of child objects as you resize the scale layout container.
    • Horizontal alignment
      . Set to
      Stretch
      to resize the scale layout horizontally when the parent container resizes.
    • Vertical alignment
      . Set to
      Stretch
      to resize the scale layout object vertically when the parent container resizes.
    • Original width
      and
      Original height
      . Determine the starting size of the scale layout object.
      IMPORTANT: The
      Original width
      and
      Original height
      properties are only visibly if you double-click the scale layout object in
      Project view
      .
      TIP: You can also adjust
      Original width
      and
      Original height
      by resizing the scale layout container in the editor.
    • (optional)
      Left margin
      ,
      Top margin
      ,
      Right margin
      ,
      Bottom margin
      . Set margins for the scale layout object.
For an example of scale layout implementation, see Scale layout
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal