Authentication properties
Property | Description |
---|---|
Default user folder | Folder that contains users created in FactoryTalk Optix Studio .
TIP:
The default folder to contain user objects is
. When a domain user logs in at runtime, a corresponding user object appears in the folder specified. |
Property | Description |
---|---|
Default user folder | Folder that contains users created in FactoryTalk Optix Studio .
TIP:
The default folder to contain user objects is
. When a domain user logs in at runtime, a corresponding user object appears in the folder specified. |
Default domain name | The default domain name for domain users that log on at runtime.
TIP:
To get the server address, enter this command in PowerShell nslookup -type=srv _ldap._tcp. , where ftoptix.local ftoptix.local is the domain name of the Active Directory server, and copy the server DNS.If you leave Default domain name blank, the domain name is set based on the Active Directory domain joined by the Windows client. |
Property | Description |
---|---|
Default user folder | Folder that contains users created in FactoryTalk Optix Studio .
TIP:
The default folder to contain user objects is
. When a domain user logs in at runtime, a corresponding user object appears in the folder specified. |
Default domain name | The default domain name for domain users that log on at runtime.
TIP:
To get the server address, enter this command in PowerShell nslookup -type=srv _ldap._tcp. , where ftoptix.local ftoptix.local is the domain name of the Active Directory server, and copy the server DNS.If you leave Default domain name blank, the domain name is set based on the Active Directory domain joined by the Windows client. |
Domain server address | Active Directory or LDAP server address.
TIP:
To get the server address, enter this command in PowerShell nslookup -type=srv _ldap._tcp.ftoptix.local , where ftoptix.local is the domain name of the Active Directory server, and copy the internet address.If you leave Default server address blank, the Active Directory server address is set based on the Active Directory domain joined by the Windows client. If you do not specify the port in the server address, the default 389 port is used. |
CA certificate file | Base64 CA certificate file.
TIP:
If you leave
CA certificate file blank, the local Windows machine is used to authenticate the user. CA certificate file is required to authenticate against a specific LDAP server or use a Linux client.
TIP:
To find items, start typing the item name to find in Select file .If the file does not appear in Select file , select ![]() Import file(s) Import file(s) , select the file to import, and then choose Select . |
Property | Description |
---|---|
Issuer | Base URL of the authentication server and issuer validator for the JSON Web Token (JWT). |
Authorization path | Authorization path on the server. For example, /oauth/authorize |
Token path | Endpoint path to get the token. For example, /oauth/token |
JWKS path | Endpoint path to get the JSON Web Key Set (JWKS). For example, /.well-known/jwks.json |
Redirect URI | Address to open in web browser on successful user login.
TIP:
The redirect URI is read as a string and is not reached by the web browser. You can use any URI.
|
Client ID | Client ID for FactoryTalk Optix project on the authentication server. |
Additional scopes | Scopes added to the default openid and profile scopes. For example, an email scope. |
Name claim | Name claim for the user name. |
Group claim | Group claim for group names in an array of strings. For example, ["group1", "group2"] |
Audience | JWT token audience where Client ID is the default. |
Provide Feedback