UI Session
Manage the idle timeout and the interactive session locale.
Properties
Name | BrowseName | DataType | Description |
---|---|---|---|
Inactivity timeout duration | IdleTimeoutDuration | Duration of the idle timeout after which the session stops. | |
Inactivity timeout active | IdleTimeoutEnabled | False: in case of user inactivity in the interface, the session remains valid; True: in case of user inactivity for a certain period of time, the session stops. | |
Events
IdleTimeoutEvent
- BrowseName
Provide Feedback