Create an organization
Organizations are collections of services, users, and resources that can be accessed and managed using FactoryTalk Hub. An organization should be as large as can be easily managed in order to maximixe economies of scale and reduce data silos.
Create an organization on your first sign-in, or from the menu at any time.
NOTE:
The user who creates an organization is the owner for that organization.
Organizations:
- can be as large as can be easily managed
- define how data and entitlements are shared by users
- can be public or private
- cannot be merged or deleted once createdNOTE: Users cannot remove themselves from the organization but owners or administrators can remove others. An administrator cannot remove access from the owner.
Complete organization details.
The following settings identify the parameters of your organization:
- Add Organization Logo- (optional) Allows you to add a graphic to help your colleagues identify the organization.
- Name(required) - Name of the organization that will be using services and SaaS provisioned for this FactoryTalk Hub. The name does not have to be unique but should be distinct and descriptive.
- OwnerName (required) - The name of the person who is responsible for administration of this FactoryTalk Hub organization.NOTE: The owner field is automatically populated by the system based on the user logged as creating the organization.
- Email Domain(required) - The email domain that identifies authorized users of this organization.NOTE: The email domain field is automatically populated by the system based on the user logged as creating the organization.
- Location(optional) - The geographic location of this organization.
- Description(optional) - A short description of the goal of the organization.
- Visibility Setting- Choose one of the two radio buttons:
- Show this organization in the public list and in search results- Other users with the same email domain can see your organization and request to join.
- Hide this organization in the public list and in search results, invite code required for members to join- No one outside your email domain can see your organization name unless you invite them.
After completing the settings for your organization, select
Create
.Provide Feedback