Connection Configuration grid
Use the Connection Configuration grid to manage parameter connections, including
adding, viewing, editing, and deleting connections.
Use the Connection Configuration grid to add, view, edit, and delete parameter
connections.
TIP:
To open the
Connection
Configuration
dialog, do one of the following:- In the Tag EditorConnectioncolumn, select the connection to view. Then selectBrowse
. - In theTag Propertiesdialog, selectOpen Parameter Connections.
Use the mouse or keyboard to navigate the
Connection
Configuration
grid.This table describes the Connection Configuration grid settings:
Setting | Description |
|---|---|
Connection | The connection endpoint. To add or edit a connection in the
Connection column:
|
![]() | Select to launch the Data Item Browser , which displays a
list of available endpoints for connections. |
Usage | The usage type of the connection endpoint (LOCAL, INPUT, OUTPUT,
or INOUT). Autopopulated.
IMPORTANT:
A single part (member,
element, or bit) of a program’s Input parameter cannot have
multiple connections.
|
Data Type | The endpoint data type, such as BOOL, SINT, INT, DINT, or REAL.
Autopopulated. |
Description | The purpose of, or latest change to, the item. Autopopulated if
available. The description, if any, for each endpoint tag or structure,
array, or bit member. |
Provide Feedback
to launch the