Upgrade a pre-shipment lineup
If a pre-shipment dataset is imported, it can be upgraded to a post-shipment dataset by
performing either:
- Overwrite. Overwrite the pre-shipment dataset with the post-shipment dataset. This option loses any changes made to the pre-shipment dataset.
- Merge. Merge the pre-shipment and post-shipment datasets. This option takes you through the lineup, highlights differences between the pre-shipment and post-shipment lineups, and lets you choose which changes to keep from either the pre-shipment or the post-shipment lineup.
To upgrade from a pre-shipment to a post-shipment lineup:
- Identify the PRE-SHIPMENT badge in either:
- IntelliCENTERexplorer at the lineup level.
- IntelliCENTER Dashboardafter the lineup name.
- In IntelliCENTER explorer orElevationview, at the lineup level, from the menu, selectUpgrade to post-shipment.
- InUpgrade to post-shipment, underDatabases, selectBrowsethen selectUpload.
- Select up to five lineups.
- SelectImport.
- InImport MCC Lineup, for each selected dataset, select any of the following and then selectNext:
- Merge differences. Merge the differences between the pre-shipment and post-shipment datasets.
- Overwrite current data with post-shipment dataset. Lose any changes to the pre-shipment dataset.
- Skip current lineup. Do not upgrade the lineup.
- If you choose to merge the differences, a wizard opens and highlights the properties that are mismatched between the two lineups. Select the main device and select eitherApply current project propertyto discard changes orKeep incoming changes propertyto keep changes.
- When all conflicts are resolved, selectImport.
Provide Feedback