Open a unit profile

Open a unit profile to view detailed information about the unit, including:
  • a list of devices contained in the unit.
  • a summary of device information, such as device name, device type, IP address, MCC Network number, vendor code, product type, product code, major revision, and minor revision.
  • current device status, if enabled.
  • links to documentation and device profiles.
  • assigned mappings for devices that support Input and Output mappings.
  • editable eight E300 Electronic Overload Relay writeable parameter values.
To open a unit profile
  1. On the explorer bar, select Devices Icon
    Devices
    .
  2. Select
    IntelliCENTER
    .
  3. In
    IntelliCENTER
    explorer, right-click a unit within a lineup and select
    Unit Profile
    .
    TIP: To open a unit profile from
    Elevation
    view, double-click a lineup and then in
    Elevation
    view, right-click a unit and then select
    Unit Profile
    .
  4. In
    Unit Profile
    view:
    • Unit documentation. Under
      Documentation
      , select the link to
      Drawings
      ,
      Manuals
      , or
      Spares
      .
    • Assigned input and output mappings for supported devices. Select the desired device at the bottom of the screen and then select the
      I/O
      tab.
      TIP: To open the full
      I/O Mapping
      view, select
      Open I/O Mapping
      .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal