View MCC lineup documentation
You can view MCC lineup documentation that was imported into a FactoryTalk Design Studio
project. View MCC lineup drawings, manuals, and spare parts, if applicable.
- InElevationview, open documentation for either a:
- Unit level. Right-click a unit to view.
- Lineup level. Right-click a blank space inElevationview.
TIP: You can also view documentation from theIntelliCENTERexplorer. Right-click either the lineup level or the unit level in the explorer. - SelectDocumentationand then select the type of documentation to review:
- Drawings. View a list of drawings associated with the MCC lineup and then double-click a drawing to download it to your local drive. Drawings are identified by file name, sheet number, path, and if the drawing is custom.
- Manuals. View a list of manuals associated with the MCC lineup and then double-click a manual to download it to your local drive. Manuals are identified by file name, publication description, publication date, path, and indicate if the manual is user-supplied.
- Spares. View a list of spare parts associated with the MCC lineup. Spare parts are identified by part number, part description, quantity required, quantity recommended on hand, category, and provide four blank columns to customize the identity of the spare part once ordered.
Provide Feedback