Import documentation

If you did not import the provided documentation when you imported an initial lineup, you can still import the documentation. You can import the documentation from either the IntelliCENTER explorer or
Elevation
view.
  1. On the explorer bar, select Devices Icon
    Devices
    .
  2. Select
    IntelliCENTER
    .
  3. In
    IntelliCENTER
    explorer, right-click either the lineup level or unit level.
    TIP: To import documentation from
    Elevation
    view, double-click the lineup name and then right-click a unit or blank space in
    Elevation
    view.
  4. Select
    Documentation > Import Documentation
    .
  5. In
    Import Documentation
    , browse to and select the folder of the Rockwell Automation documentation to import.
  6. Select
    Import
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal