Import new sections
Import sections to add sections to existing lineups.
- Either:
- In theIntelliCENTERexplorer, right-click the lineup.
- InElevationview, right-click empty space.
- SelectImport Sections.
- InImport Sections, underDatabasesnavigate to the dataset folder on your local drive.
- To import new section documentation, underDocumentation, selectBrowseto navigate to the folder on your local drive.
- SelectUploadtwice.
- With the files to import selected, selectImport.The data files import into FactoryTalk Design Studio and appear at the end of the lineup.
- (optional) To rearrange sections, drag sections to their new locations.
Provide Feedback