Elevation view components

Elevation
view is a digital representation of the physical Motor Control Center hardware.
Item
Description
Lineup
Custom grouping of MCC hardware comprised of devices, units and buckets, and sections and /columns
Section
vertically stacked grouping of units within a Motor Control Center
Unit
Box that electrically and physically plugs into the Motor Control Center that contains devices that have been installed and wired in manufacturing. For units in error, a warning code appears with a number returned from certain devices that indicates the reason for the device fault. For unit warning code definitions, refer to device user manual.
Unit location
Number and letter that indicates the physical location within the Motor Control Center. The Number indicates section/column counting from left to right and the letter indicates the vertical position within the section/column.
Door
A door unit represents empty space within an MCC that is covered by a door. A door can be replaced with a unit only dataset.
Dual Unit
A unit that is internally divided into a left and right section. The unit shares a single door. The unit and door can only be moved together. The dual unit is only available in the CenterLine 2100.
Wireway
Horizontal empty space at the top and bottom of every section or column of a Motor Control Center. Use a wireway to run wires or an Ethernet switch.
Device
Components within a unit or bucket. If a unit contains more than one device, the primary device details appear on the unit. Double-click a unit to open the primary device profile.
TIP: For Motor Control Center product families use different names for the components, both names appear in the
Item
column.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal