Edit the MCC lineup

In
Elevation
view, move sections and units within the same section. You can exchange units with doors and units from other sections to match changes made to the physical MCC. You must exchange units of the same size. Moving wireways or units into wireways is not permitted.
  1. In
    Elevation
    view, select the unit or section to move.
  2. Drag the unit up or down within the same section or drag the unit to a new section. Move sections forward or backward to a new section location.
    TIP: Dragging a unit within a section displays a green line at the bottom of the dragged unit to indicate that the new location is permitted. A unit is outlined in green when you drag the unit to a permitted location. The unit is outlined in red when you drag the unit to a location that is not permitted.
    TIP: When moving a unit into a door, if the unit is smaller than the door,
    Move Unit
    opens for you to move the unit to the top or bottom of the door. The resulting smaller door appears where indicated, and a new door the same size as the moved unit appears in the original location of the unit.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal