Set the device path
Use
Deploy center
to set, modify, or clear the device path that specifies the target
controller for the deploy operation.To set the device path
- On the explorer bar, select
Open the deploy center tab.NOTE: You can also selectDeploy centerat the bottom of theDevicesexplorer. - InDeploy center, in thePathcolumn, select
, and then
select Controller path. - InSet device path, expand the target FTRA_VPN endpoint, right-click the controller, and then selectConnect.TIP: If you are connecting to the FTRA_VPN endpoint for the first time or have added a device, you may need to reconnect to the FTRA_VPN endpoint to see the controller under the FTRA_VPN endpoint.
- Expand the FTRA_VPN endpoint and then select the controller.
- SelectOK.TIP: You can manually edit the device path.
The selected communication path is saved as the current device
path.
Provide Feedback