Redeploy a project

Redeploy a project to deploy that project to a different controller. Change the controller path and add or change the comment about the redeployment.
  1. On the toolbar, select Deploy icon
    Open the Deploy center tab
    .
  2. In the grid on
    Deployment History
    , select the project to redeploy.
  3. Select
    Re-deploy
    .
  4. For each controller in
    Set device path and add comment
    , change the entries in these columns:
    • Path
      . Enter the new IP address of the controller.
    • Comment
      . Add or edit the comment for the redeployment of the controller.
    TIP: The
    Controller application
    column is read-only and displays controllers selected on the
    Re-deploy
    tab.
  5. Select
    Re-deploy
    .
The project redeploys to the updated controller path.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal