Safety Instructions

Use safety instructions to build logic for use in safety applications.
Available instructions
If you want to:
Use this instruction:
Control and monitor redundant outputs.
Monitor dual-input safety devices whose main function is to stop a machine safely. An E-stop, light curtain, or safety gate are examples of dual-input safety devices.
Monitor a locked feedback signal from a dual-input safety device and issue a lock request to it.
Monitors dual-input safety devices and set O1 (Output 1) based on the Input Type operand and the combined state of Channel A and Channel B.
Indicate, through O1 (Output 1), if the safety mat is occupied.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal