Loading
Press Release
Recent ActivityRecent Activity

Rockwell Automation Introduces Next Generation Edge Gateway to Accelerate IT/OT Convergence

FactoryTalk® Edge Gateway™ accelerates edge to cloud digital transformation and unlocks higher value business insights at enterprise level

Share This:

LinkedInLinkedIn
TwitterTwitter
FacebookFacebook
PrintPrint
EmailEmail
Main Image
Press Release
Recent ActivityRecent Activity
Rockwell Automation Introduces Next Generation Edge Gateway to Accelerate IT/OT Convergence
FactoryTalk® Edge Gateway™ accelerates edge to cloud digital transformation and unlocks higher value business insights at enterprise level

Share This:

LinkedInLinkedIn
TwitterTwitter
FacebookFacebook
PrintPrint
EmailEmail

Today, Rockwell Automation introduced the first capability of its edge strategy with FactoryTalk Edge Gateway, to simplify and accelerate IT/OT convergence. Industrial enterprises struggle to aggregate operational data from heterogeneous sources and add relevant context from the source—such as process conditions, time stamps, machine states and other production states—to the IT layer. This prevents them from uncovering potentially game-changing insights at the enterprise level. While traditional gateway solutions fail to address these important challenges, FactoryTalk Edge Gateway goes a step above to not only enrich OT data with critical context where it matters the most—at the edge—but also delivers it in a flexible common information model to IT applications, so that industrial enterprises can derive critical insights for a competitive edge.

FactoryTalk Edge Gateway is an important foundation of a broader edge platform offering that will include elements of pre-built data analytics models, machine learning, tailored applications, and scalable compute. It is the latest addition to the highly recognized and widely adopted FactoryTalk® Analytics suite offering that addresses diverse industries and Industrial IoT (IIoT) use cases. FactoryTalk Edge Gateway is also a key pillar in Rockwell Automation’s strategy to accelerate digital agility across the industrial devices to cloud spectrum with partnerships, including PTC and Microsoft.

Today, industrial facilities are made up of heterogeneous systems and devices that generate voluminous data at very high speeds—resulting in significant data silos. Connecting the dots across these industrial data silos by building relevant OT data context is critical for generating higher value actionable insights. Furthermore, unless the industrial OT data is packaged into a logical data model that both IT and OT applications can understand, IT/OT convergence remains a farfetched prospect.

A leading Fortune 100 pharmaceuticals manufacturer says, “Legacy systems today are not IIoT enabled and need many different software programs to collect and organize data. With existing methods, the operational attribute values collected have different timestamps, so it is impossible to synchronize the data together. Compared to that, FactoryTalk Edge Gateway automatically stitches the data together and puts it in a payload using pre-configured information model hierarchy. It gives one solution to collect and organize the relevant data.”

FactoryTalk Edge Gateway’s unique data management capabilities result in up to a staggering 70% reduction in analytics data preparation efforts for data scientists or analysts, while providing higher quality OT data. The underlying common information data model is orchestrated by the unique Rockwell Automation FactoryTalk® Smart Object™ capability and can be efficiently mapped to on-premises or cloud applications to generate predictive insights across the enterprise. FactoryTalk Edge Gateway is designed to integrate with best-in-class ecosystem solutions like Microsoft Azure and FactoryTalk® InnovationSuite™, powered by PTC, and a variety of big data, IIoT, and cloud applications.

“Industrial businesses need actionable enterprise-level insights to achieve their goals. As customers continue to drive IT/OT integration and leverage operational data to drive insights, they are realizing that having the right OT data context is critical to scale their digital transformation initiatives,” said Arvind Rao, Director, Product Management for Information Systems at Rockwell Automation. “With FactoryTalk Edge Gateway, we are dramatically reducing the time and effort required to build, maintain and enrich this critical OT context. This provides our customers with the opportunity to realize double-digit operational improvements through analytics.”

Published October 27, 2020


Subscribe

Subscribe to Rockwell Automation and receive the latest news, thought leadership and information directly to your inbox.

Subscribe

Recommended For You

Loading
  • Sales
  • Customer Care
  • TechConnect Support
  • General Questions
  1. Chevron LeftChevron Left Home Chevron RightChevron Right
  2. Chevron LeftChevron Left Company Chevron RightChevron Right
  3. Chevron LeftChevron Left News Chevron RightChevron Right
  4. Chevron LeftChevron Left Press Releases Chevron RightChevron Right