Presenter
Discover how companies use modular systems’ high degree of freedom worldwide. With the modular system, the choice of electrical components is completely up to you. The versatility regarding width, height and depth means that the panel can be designed to suit its place of installation, and ensures simultaneously that the panel can be modified or extended. The system is fully documented and is supplied as flat-pack worldwide to panel builders, who construct and offer complete panel systems. All panel builders have gone through extensive training/education to ensure a high and uniform quality level all over the world on panel systems enclosed with the CUBIC modular system. CUBIC has many years of experience in delivering enclosure solutions based on our modular system that is applicable in several industries.
During this webinar, we will explore the advantages of using CUBIC Modular System. The MODULAR SYSTEM gives integrators the freedom to assemble any kind of motor control center. The philosophy behind the signature IEC enclosure system makes it possible for integrators to build every type of motor control solution in the low-power segment, based on several standard parts, without compromising on quality.
Our specialists will show how system integrators can successfully inherent part of the modular idea which is the freedom to choose power components from any supplier. This allows for the construction of just the right motor control center based on customer requirements. On top of the versatility of the modular system it is also one of the safest and most tested enclosure systems on the market.
In this webinar you will learn:
- The power of modularity - the innovative approach to the CUBIC modular system offers the utmost flexibility to design and build electrical switchboard and motor control centers to meet your most demanding specifications.
- Being independent - the brand agnostic approach allows you to design the system that best fits your needs.
- Certification advantages - CUBIC modular enclosure systems are tested and verified by the worlds most recognized test laboratories.
- Partner Network – you can join our CUBIC Modular Assembly partner capability
- Training Support - An extensive education and training program along with global support for authorized providers helps ensure deliver of high-quality packaged solutions