Replace a Redundant Module

To replace a redundant module, refer to one of the following procedures in Module Replacement:
  • Perform a direct module replacement in the secondary chassis
  • Perform a communication module series replacement
  • Perform a redundancy module catalog number replacement
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal