Obtain the Redundancy Module Configuration Tool
The
FactoryTalk® Linx
Redundancy Module Configuration Tool (RMCT) enables online operation and configuration of ControlLogix®
redundancy modules. You must use the RMCT with ControlLogix®
5590 controller systems. For compatible versions of the
FactoryTalk® Linx
RMCT with your redundancy system, see the release notes for your redundancy bundle or redundancy module on the Product Compatibility and Download Center (PCDC) at rok.auto/pcdc.There are multiple ways to obtain the
FactoryTalk® Linx
RMCT:- Download from the PCDC.
- Download as part of theStudio 5000 Logix Designer®application.
For details about obtaining the RMCT, see the Knowledgebase Technote
Redundancy Module Configuration Tool (RMCT)
.Provide Feedback