Requested Packet Interval (RPI)

The RPI for I/O connections in a redundant-enabled controller tree is configured the same way as with a simplex controller. The RPI rates of I/O connections impact the loading of the associated
EtherNet/IP
communications modules. The RPI can be the same as a non-redundant chassis.

1756-EN4TR Module Considerations

For all communication module catalog numbers beginning with 1756-EN4TR, keep the RPI rate for I/O connections such that the I/O packet rate is under 80% of the maximum (50,000 packets/second).

1756-EN2T Module Considerations

This table describes CPU usage considerations for all communication module catalog numbers beginning with 1756-EN2T.
CPU Utilization Percent
Action
0…80%
No action is required.
Important: This range is the optimal rate.
Greater than 80%
Take steps to reduce your CPU utilization.
  • Adjust the RPI of your connections.
  • Reduce the number of devices that are connected to your module.
  • Add another communication module to the redundant chassis pair (7, max)
IMPORTANT: Your communication module can function at 100% CPU capacity, but at or near this rate, you run the risk of CPU saturation and performance degradation.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal