Other Memory Card Tasks
You can perform these tasks with the memory card:
- Change the image that is loaded from the card
- Check for a load that was completed
- Clear an image from the card
- Store an empty image
- Change load parameters
- Read/write application data to the card
- View safety-lock status and safety signatures on the Nonvolatile Memory tab
For more information on how to complete any of these tasks, see the Logix 5000 Controllers Memory Card Programming Manual, publication 1756-PM017.
Provide Feedback