Windowxx View
Windowxx shows a specific module windows configuration.
Windowxx View Example

The Windowxx view includes these parameters:
Parameter | Description |
---|---|
Window Mode | Displays the mode that the window is configured for. |
Output On Value | Displays the value that defines one side of the window
thresholds. The outputs (if tied to the window) and
I.Windowxx.InWindow tag switch state at this
threshold according to the diagram Figure 1. |
Output Off Value | |
Output On Hysteresis | Displays the negative offset from the Output On Value to apply
hysteresis to. |
Output Off Hysteresis | Displays the negative offset from the Output Off Value to apply
hysteresis to. |
Outputs Controlled by this Window Output00 | Determines whether this window controls the indicated output. |
Outputs Controlled by this Window Output01 | Determines whether this window controls the indicated output. |
Provide Feedback