Time Synchronization View
The Time Synchronization view is read-only and displays the CIP Sync status information
about the module when the project is online. Time Synchronization displays the following
information:
- CIP Sync time synchronization status
- UTC system time
- Grandmaster Clock information
- Grandmaster Clock description
- Local Clock information
Time Synchronization View Example

Grandmaster Clock Description
The Grandmaster clock description dialog provides detailed information about the
grandmaster clock.
To view the Grandmaster clock description, select Description in the Time
Synchronization view.
Grandmaster Clock Description Example

Provide Feedback