Input View
Use Input to view or configure the input for the device.
Input View Example

The Input view includes these parameters:
Parameter | Description |
---|---|
Input | Displays the Input number to which this configuration
applies. |
Input Filter Time Off → On | Defines how long an Off to On input transition must remain in the
On state before the device considers the transition valid. |
Input Filter Time On → Off | Defines how long an On to Off input transition must remain in the
Off state before the device considers the transition valid. |
Diagnostics | Opens the Diagnostics dialog, which contains diagnostic
information. |
Input00 Diagnostics
To view the Input00 diagnostics, select Diagnostics in the Input view.
Input00 Diagnostics Example

Provide Feedback