Connection View

Use Connection to define controller-to-device behavior:
  • Set the RPI rate. For more information, see Requested Packet Interval.
  • Select Unicast or Multicast connection to use on the EtherNet/IP network. For more information, see Unicast or Multicast Connection.
  • View the reason of Connection Fault.
    TIP: If there is a connection fault, Connection Fault area displays the error code with description that helps you to troubleshoot the module. For more information, see Troubleshoot Your Module.
  • Inhibit the module. For more information, see Module Inhibiting.
  • Configure fault response for connection failure while the controller is in Run Mode.
  • Enable or disable the Automatic Diagnostics.
    ATTENTION: If you do not enable Automatic Diagnostics, the device does not publish diagnostics to FactoryTalk Alarms and Events.
Connection View Example

Recommended Minimum RPI Values for Notch Filters

In the following table, each Notch Filter setting has two recommended minimum module RPI values that allow the required time to collect samples from each channel. One setting provides faster sample speed and the other provides slightly better resolution at slower sample speeds.
Notch Filter and Recommended Minimum Module RPI Values
Notch Filter (Hz)
Recommended Minimum Module RPI Value
Application That is Configured With Only One Channel Enabled
Application With All Channels Enabled and Using the Same Notch Filter Setting on All Channels
Faster Sampling Speed
(ms)
Better Noise Rejection
(ms)
Faster Sampling Speed
(ms)
Better Noise Rejection
(ms)
10
106
316
422
NA
20
53.1
158.1
212
632
50
22
64
86
254
60 (default)
18.3
53.2
72
212
100
11.2
32.1
44
127
200
5.9
16.4
22.2
65
400
3.5
8.6
12
33
500
2.8
6.9
9.3
26.5
1000
1.7
3.8
5.2
13.5
5000
1.0
1.3
2.2
3.3
10000
0.7
0.9
1.7
2.1
15625
0.8
0.8
1.7
1.7
31250
0.4
0.6
1.2
1.5

Minimum RPI Calculation When Using Different Notch Filter Selections

When input channels on the same module use different Notch Filter selections, you must consider the sample time for each channel. This helps you to find the recommended RPI that provides enough time for sampling all channels.
Because all input channels in 5034-IF4 share the same Analog to Digital Converter, the recommended minimum RPI rate for all enabled channels added together is the recommended minimum module RPI.
Example Application That Requires Faster Sampling Speed
Channel
Notch Filter (Hz)
Recommended Minimum Module RPI for Each Channel (ms)
Recommended Minimum Module RPI (ms)
Ch00
50
22
24.1
Ch01
1000
1.7
Ch02 - Disabled
N/A
N/A
Ch03
31250
0.4
Example Application That Requires Better Noise Rejection
Channel
Notch Filter (Hz)
Recommended Minimum Module RPI for Each Channel (ms)
Recommended Minimum Module RPI (ms)
Ch00
50
64
68.4
Ch01
1000
3.8
Ch02 - Disabled
N/A
N/A
Ch03
31250
0.6
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal