Resume updates to a trend chart
A paused trend chart does not update traces. No data plots for the time span when the trend chart pauses. Resume updates to a trend chart to plot data and update traces. When updates resume, the trend chart plots data collected during the pause.
To resume updates to a trend chart
- At the bottom of the trend chart, selectResume
. Updates to the trend chart resume and data updates are plotted on the traces.
TIP:Tips:- The HMI Designer determines if a button appears to interact with the trend chart on the HMI device.
- To use the HMI device keypad or an external keyboard to press a button on the trend chart, tab to the button and pressEnter.
Provide Feedback