Web browser
Use the web browser to access content on the intranet, the Internet, remote file servers, devices with built-in web pages, removable SD or USB drives, or IP cameras.
You can only access the web browser through a command defined in the HMI application. Your level of access depends on the security configuration and your account privileges.
You can run only one instance of a web browser at a time. To run a different instance of the web browser, first close the running instance. The web browser supports only one window or tab at a time. Links that open a page in a new tab or new window may not function. Bookmarks, file downloads and uploads are disabled. The HMI device does not retain browsing history, login data, or cookies.
While using the web browser, pressing the Navigation button, navigating to a different screen, or opening a popup closes the browser window. You can also close the web browser using a Close Web Browser command. The Close Web Browser command discards any data not committed to the web page, such as data entered into forms, or text boxes.
IMPORTANT:
An open web browser captures all key presses. Project events relying on key presses do not trigger when the browser is open.
On high RAM memory use, the web browser closes the open web page and displays an error dialog so that you can reload the web page or close the browser.
If the HMI application has Auto-Logoff enabled, the browser closes. Playing videos and accessing IP cameras does not prevent auto-logoff unless the user performs other activities.
Provide Feedback