Cancel the export of a data log
Cancel the export of a data log to stop creating the export file for the data log and not save it to removable media. Cancel the export when the data log for the current project is exporting to the USB storage device or SD card in the HMI device.
To cancel the export of a data log
- Open theSettingsscreen.
- SelectData Export. TheData Exportpopup opens, showing the progress of the export.
- SelectCancel. The progress indicator stops to indicate the export is cancelled.
Provide Feedback