Set the date and time on the HMI device
The HMI device has a default date, time, and time zone. Change the values using the
Date and Time
popup. To set the date and time on the HMI device
- On the HMI device or in theSystem Banner, selectNavigation
and then select Settings. - SelectDate and Time. TheDate and Timepopup opens.
- In theDatebox,enter the month, day, and year in MM/DD/YYYY format and selectOK.
- In theTimebox,enter the hours, minutes, and seconds in HH:MM:SS format and selectOK.
- In theTime Zonebox, scroll to and select the time zone.
- SelectClose
.TIP:PanelView5000 HMI devices contain a built-in database of all daylight savings time rules.PanelView5000 switches to daylight savings time automatically according to the selected time zone.
Provide Feedback