Disable downloads to the HMI device
Downloads to the HMI device are enabled by default. Disable downloads to the HMI device as a security measure. This prevents replacing the current application when downloading an application from
View Designer
. The Allow downloads and Firmware Updates
option applies to downloads,
ControlFLASH™
, and Reset Service requests. To disable downloads
- On the HMI device or in theSystem Banner, selectNavigation
and then select Settings. - SelectHMI Device. TheHMI Devicepopup opens.
- ClearAllow downloads and Firmware Updates. Project downloads to the HMI device are now denied.TIP:SelectAllow downloads and Firmware Updatesto download another project.
- SelectClose
.
Provide Feedback